0
0 ItemsHK$0.00

Uninterruptible Power Supply (UPS) Systems for Critical Loads in Smart Buildings

In modern smart buildings, where automation, connectivity, and critical infrastructure rely on a steady power supply, even a brief outage can disrupt essential operations

Block diagram of critical loads in a smart building

An Uninterruptible Power Supply (UPS) safeguards vital systems such as emergency lighting and security networks, by ensuring continuous power during blackouts, voltage fluctuations, and surges. This article elaborates on the important considerations of UPS selection such as critical loads in smart buildings and the different kinds of UPS systems suited for these environments. The use of an appropriate UPS ensures efficiency, reliability, and resilience.

Critical loads: Lifelines of smart buildings

Critical loads in a smart building require uninterrupted power to maintain safety, security, and essential operations. These vital electrical loads include fire detection systems, emergency illumination, security infrastructure, and, often, the building management system (BMS). The consequences of failure are severe: a non-functioning fire alarm could impede safe evacuation, while disabled security systems might leave occupants vulnerable, and a server reboot might take minutes, but the resulting data loss or service interruption could cost thousands of dollars per second in a data-driven facility. The supply of power must be constant as outages-whatever the duration- threaten lives, halt business continuity, and trigger significant financial damage. Unlike non-essential systems like regular lighting or comfort-focused HVAC, critical loads must remain uninterrupted to ensure the building functions appropriately. The types of Critical Loads in Smart Buildings are:

  • Life safety systems: These are crucial for occupant safety during emergencies and include fire alarms, emergency lighting, and sprinkler systems.
  • Security systems: Access control, surveillance cameras, and other systems ensure building security, especially in hospitals, airports, and other critical buildings.
  • Communication systems: Critical systems rely on telecom and internet services for constant connectivity, which are vital for operational continuity or discharging emergency responses.
  • Elevators and escalators: Essential for accessibility and evacuation in skyscrapers, often connected to the BMS in smart buildings.
  • Critical IT infrastructure: Servers and data centers hosting essential applications, such as electronic health records in smart hospitals or operational data in smart offices.
  • Building management system (BMS): If the BMS controls other critical systems, it may be considered a critical load due to its role in monitoring UPS and other essential functions.
Block diagram of offline/Stand-by UPS topology

Figure 1: Block diagram of critical loads in a smart building

Types of UPS systems for smart buildings:

Modern UPS systems are divided into three main categories, each offering different levels of power protection: offline, Line-Interactive, and Online.

  • Offline/Standby UPS: An offline (standby) UPS provides essential power protection by supplying electricity directly from the mains during regular operation. The battery is kept fully charged by the battery charger while the inverter remains idle. Fluctuations in power or a power failure results in the relay switching the load to the inverter. This switch activates after a short 10-20 ms delay to supply backup power. This UPS type offers affordable protection with minimal complexity and is best suited for non-critical loads like PCs and standalone office equipment. However, the brief switchover time may not be ideal for highly sensitive systems in smart buildings.

Block diagram of Line-Interactive UPS topology

Figure 2: Block diagram of offline/Stand-by UPS topology

  • Line-Interactive UPS: Provides intermediate-level power protection by combining voltage regulation with backup power. It is different from an offline UPS as it continuously conditions the AC mains, adjusting for voltage fluctuations to deliver a stable output. If mains power is available, the inverter continues to be connected to the load and operates in reverse mode to charge the battery. During an outage, the system seamlessly switches to battery power with minimal transfer delay, reducing switching transients. This design makes line-interactive UPS ideal for enterprise networks, IT infrastructure, and office environments, offering improved protection over offline systems while remaining cost-effective.

Block diagram of Online/double conversion UPS topology

Figure 3: Block diagram of Line-Interactive UPS topology

  • Online/Double Conversion UPS: An online (double conversion) UPS provides the highest level of power protection by continuously converting incoming AC power to DC and then back to AC, ensuring a stable and clean output. Unlike offline and line-interactive UPS systems, it eliminates transfer time during power failures, as the batteries always supply power to the inverter. This design is ideal for those that require 100% uptime, such as for sensitive equipment and critical applications. While the double-conversion process reduces efficiency, advanced models minimise energy loss by optimising power flow. Online UPS systems are the preferred choice for data centers, medical equipment, and industrial automation, where even minor power disturbances can cause significant disruptions.

Figure 4: Block diagram of Online/double conversion UPS topology

Hence, we can conclude that Online UPS systems are the best solution for critical loads in smart buildings because they provide seamless and uninterrupted power, ensuring zero switching delays during input failures. The inverter in an online UPS is always active, making it different from other types of UPS. The online UPS inverter delivers a consistent and high-quality power supply to sensitive equipment. The system instantly switches to battery power without delay if the AC power is interrupted, protecting critical devices from uninvited disruptions. Additionally, reliability gets a boost if a battery energy storage system (BESS) is integrated with a bidirectional charger.

FeatureOffline UPSLine-Interactive UPSOnline UPS
Working PrinciplePowers load directly from mains; switches to battery during power issuesInverter always connected; regulates voltage and provides battery backup as neededContinuous double conversion; isolates equipment from power issues
Transfer Time to BatteryTypically, 2-10 milliseconds.Typically, 2-4 milliseconds.None (zero transfer time).
Voltage ConditioningMinimal; limited protection against power irregularitiesModerate; can correct under and over-voltage conditions without using batteryHigh; provides clean and stable power regardless of input quality
EfficiencyHigh (typically 95-98%)High (typically 90-96%)Lower (typically 80-90%) due to continuous double conversion
Surge/Noise ProtectionProvides basic surge suppression and line noise filteringOffers basic surge suppression and noise filtering, similar to Offline, but enhanced by AVR for better voltage stabilitySuperior protection, as double-conversion isolates equipment from surges, noise, and other AC line disturbances
CostLowMediumHigh
Typical Applications in Smart BuildingsPC Home, Internet workstations, Telephone switchboards, Tills, POS terminals, Fax machines, small groups of emergency lights Industrial and domestic automationCorporate computer networks, Security systems, Emergency systems, Lighting systems, Domestic and industrial automationCorporate IT network, Telecommunications, Electromedical sector, Industrial automation, Emergency systems, Protection of dedicated lines, Critical industrial/civil applications, Upstream of power-supply units, Any other possible application

Table 1: Comparison table summarizing the key points of Offline UPS, Line-Interactive UPS, and Online UPS

Design considerations for UPS in smart buildings

Smart buildings require careful planning - here are the key design factors to consider when evaluating your specific needs.

  • Power quality: Match the UPS output to the load's tolerance. Sensitive electronics need pure sine wave output, while less critical devices may handle modified sine waves. Monitor total harmonic distortion (THD)—so it does not exceed 5% for optimal performance.

  • Load analysis: Calculate the total power demand of critical loads in watts or volt-amperes (VA). Add a 20-30% safety margin for future expansion or inrush currents. For example, a server rack drawing 2 kW requires a UPS rated for 2.5-3 kVA.

  • Availability and battery runtime: The actual runtime needs must be found, as this influences the solution cost. The four basic configurations are:

    1. UPS with 10-15 minutes runtime without generator (covers 90-95% of outages)
    2. UPS with 10-15 minutes runtime with generator (reliable setup for most situations)
    3. Redundant UPSs with generator and dual power feeds (highest reliability)
    4. UPS with 2+ hours battery runtime (when generators aren't practical)
  • Form factor: Consider space requirements and installation location to determine whether a tower or rackmount model is better suited for your environment. Some UPS units offer 2-in-1 form factors.

  • Scalability: Scalable UPS solutions enable cost-effective capacity increases. Use N+1 or 2N configurations for high-reliability applications. An N+1 setup adds one UPS module beyond the minimum required, while 2N provides a fully mirrored system. For example, a 100 kVA critical load with N+1 might use two 100 kVA UPS units, ensuring failover capacity.

  • Integration with smart systems: Equip UPS units with communication protocols such as SNMP or Modbus, enabling the BMS to monitor real-time battery health, runtime, and load status. Advanced systems even predict failures using AI-driven analytics.

  • Manageability: Power management software ensures work is saved and equipment shuts down gracefully during extended outages. Consider additional capabilities such as:

    1. Power event notifications (emails, alerts, texts)
    2. Event logging
    3. Integration with virtual environments (VMware, Hyper-V, Nutanix)
    4. Battery monitoring and service notifications
    5. Remote monitoring by manufacturer service personnel
  • Budget: Balance performance features against cost constraints by prioritizing needs for redundancy, scalability, efficiency, software management, modularity, and serviceability.

Conclusion

A reliable UPS is more than a backup system. It is crucial to maintain power stability as smart buildings continue to integrate IoT, automation, and renewable energy. A well-designed UPS shields essential infrastructure from voltage outages, surges, and power fluctuations, from hospitals and data centres to security and automation systems. Investing in the right UPS system minimises downtime, safeguards productivity, and prevents costly disruptions.

Applications

Internet of Things

Internet of Things

Artificial Intelligence

Artificial Intelligence

Industrial Automation & Control

Industrial Automation & Control

Transportation

Transportation

Healthcare

Healthcare

Robotics

Robotics

Maintenance & Safety

Maintenance & Safety

EV Charging

EV Charging

Further Resources

Calculators & Conversion Charts
Selection Guides and Catalogues
Essential Learning Modules
Tech Spotlights
Design Resources
Engineering Glossary
Technical Support
Parts Finder Tools